DIN#.INV

Description

Sets or gets the polarity of a digital input.

Value

Description
0 – Active High The digital input state is 1 when voltage is applied to the I/O pin
1 – Active Low The digital input state is 1 when voltage is removed from the I/O pin

Examples

Code

With 24V on DIN1:

--> DIN1.INV 0 //Active High
--> DIN1.STATE 1 --> DIN1.INV 1 //Active low --> DIN1.STATE 0

With 0V on DIN1:

--> DIN1.INV 0 //Active High
--> DIN1.STATE 0 --> DIN1.INV 1 //Active low --> DIN1.STATE 1

Context

For more information see Digital Inputs and Outputs.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units N/A
Range 0 to 1
Default Value 0 (Active high)
Data Type Integer
See Also  

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable

DIN1.INV

3590h

01h

Unsigned8

-

-

Read/Write

No

DIN2.INV

3591h

01h

Unsigned8

-

-

Read/Write

No

DIN3.INV

3592h

01h

Unsigned8

-

-

Read/Write

No

DIN4.INV

3593h

01h

Unsigned8

-

-

Read/Write

No

DIN5.INV

3594h

01h

Unsigned8

-

-

Read/Write

No

DIN6.INV

3595h

01h

Unsigned8

-

-

Read/Write

No

DIN7.INV

3596h

01h

Unsigned8

-

-

Read/Write

No

DIN8.INV

3597h

01h

Unsigned8

-

-

Read/Write

No

DIN9.INV

3598h

01h

Unsigned8

-

-

Read/Write

No

DIN10.INV

3599h

01h

Unsigned8

-

-

Read/Write

No

DIN11.INV

359ah

01h

Unsigned8

-

-

Read/Write

No

DIN12.INV

359bh

01h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

DIN1.INV

20050

4E52

Unsigned8

Read/Write

-

DIN2.INV

20051

4E53

Unsigned8

Read/Write

-

DIN3.INV

20052

4E54

Unsigned8

Read/Write

-

DIN4.INV

20053

4E55

Unsigned8

Read/Write

-

DIN5.INV

20054

4E56

Unsigned8

Read/Write

-

DIN6.INV

20055

4E57

Unsigned8

Read/Write

-

DIN7.INV

20056

4E58

Unsigned8

Read/Write

-

DIN8.INV

20057

4E59

Unsigned8

Read/Write

-

DIN9.INV

20058

4E5A

Unsigned8

Read/Write

-

DIN10.INV

20059

4E5B

Unsigned8

Read/Write

-

DIN11.INV

20060

4E5C

Unsigned8

Read/Write

-

DIN12.INV

20061

4E5D

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

DIN1.INV

20050

Unsigned8

Read/Write

-

DIN2.INV

20051

Unsigned8

Read/Write

-

DIN3.INV

20052

Unsigned8

Read/Write

-

DIN4.INV

20053

Unsigned8

Read/Write

-

DIN5.INV

20054

Unsigned8

Read/Write

-

DIN6.INV

20055

Unsigned8

Read/Write

-

DIN7.INV

20056

Unsigned8

Read/Write

-

DIN8.INV

20057

Unsigned8

Read/Write

-

DIN9.INV

20058

Unsigned8

Read/Write

-

DIN10.INV

20059

Unsigned8

Read/Write

-

DIN11.INV

20060

Unsigned8

Read/Write

-

DIN12.INV

20061

Unsigned8

Read/Write

-